MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS2DE12 current draw

I am using a LIS2DE12 however I can't get the current on the VDD_IO to drop below 25uA.Is there any reason for this?My current settings are:CTRL_REG1 = 0x3FCTRL_REG2 = 0x30CTRL_REG3 = 0x40INT1_CFG = 0x0AINT1_THS = 0x25I am running off a 3V supply.Che...

GRose.2 by Associate
  • 1012 Views
  • 1 replies
  • 0 kudos

Resolved! I'd like to read the answers to a community question.

Specifically,https://community.st.com/s/question/0D50X00009XkXz9SAF/lis3dh-interrupt-int1-mode-not-firingI'm loged in but all that is shown is the question and a notice that the "This question is closed."Does that mean the question was never answered...

JMatt by Associate II
  • 1822 Views
  • 3 replies
  • 0 kudos

Resolved! LPS33WTR Interrupt control

Hi,In the LPS33WTR pressure sensor,I want to program the LPS33WTR FIFO to a certain pressure and configure the interrupt as Threshold-based interrupt.No Where have I found the duration of the Interrupt logic change. I want to use it as a HW trigger o...

SGano.1 by Associate II
  • 2534 Views
  • 4 replies
  • 0 kudos

How to read PDM microphone with the Serial Audio Interface(SAI)

I have a really simple application setup. I'm currently feeding in one PDM microphone. I'm using the SAI interface (code is attached). First there appears to be a bug in the ST code. The SAI_PDMCR register have a field to set up to 4 microphones (see...

nlbutts by Associate II
  • 2380 Views
  • 2 replies
  • 0 kudos

Vibration Monitoring example code works fine with FFT size of 512. But does not work with FFT size of more than 512.

We are using X-Nucleo-IKS02A1 board to test the vibration sensor using vibration monitoring example code. The FFT data of vibration sensor is observed using Unicleo-GUI.It is observed that the FFT data is not represented in Unicleo-GUI when FFT size ...

Rajesh1 by Associate II
  • 3439 Views
  • 7 replies
  • 0 kudos