MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

IIS328DQ value freeze after software reset

In my application I read out the sensor values (register 0x20-0x2D) with an interrupt every 20ms. After a software reset I have the strange behaviour that the acceleration value of the X-axis stops at a certain value (somewhere in the range of the cu...

0693W000006HOppQAG.png 0693W000006HOvsQAG.png 0693W000006HOvxQAG.png 0693W000006HOwRQAW.png
SThei.1 by Associate
  • 1609 Views
  • 2 replies
  • 0 kudos

How to change LIS3DSH resolution

Hello everyone, I am new to STM32 and to Keil. I would like to change the accelerometer resolution from 2G to 16G, but due to my inexperience, I don't know how. My teacher didn't help my and said that I need to figure it out by myself, but I really d...

TrixCZE by Associate II
  • 1335 Views
  • 1 replies
  • 0 kudos

VG6640 image sensor streaming questions.

Hello. I just start to work with vg6640 image sensor. According to the datasheet all what i need to do make it start streaming is to make sensor into STREAMING state. I have done that, the SystemFsm register shows that i'm in the SENSOR_STREAM state ...

AYako.2 by Associate
  • 1779 Views
  • 2 replies
  • 0 kudos

How to distinguish the IC?(LIS2DW12&IIS2DLPC)

Hi, I have purchased several three-axis acceleration chips, but I mixed them together by mistaken. The chip is too small, and I can’t see if there is any text on them to distinguish them. After comparing the chip manuals of both , It seems to be ind...

Xxia.1 by Associate II
  • 2972 Views
  • 6 replies
  • 0 kudos

Resolved! GPIO / EXTI interrupts, STOP2 mode and H3LIS331DL

I've got erratic behavior of access to H3LIS331DL sensor from my MCU when STOP2 mode is set. It seems that sometimes, the Interrupt ( INT1 on DRDY) received from theH3LIS331 is not, or very lately processed (maybe after wake up from other reason). I...

PGoud by Associate III
  • 1896 Views
  • 4 replies
  • 0 kudos

Resolved! Can I please know, How to interface MKI196V1 (ASM330LLH) with Raspberry Pi? Are any Python packages available? I tried I2C with raspberry but doesn't return sensor values. Also, SPI support is not available.

I am trying to build a project 'GPS aided INS' in college. I have tried many options for interfacing  "MKI196V1 (ASM330LLH)" IMU, but couldn't get the results. I tried interfacing the sensor with STM32 (maple mini) using sduino, also with nano and u...

STM32F4 Discovery I2C LIS3DSH Problem

I have tried to work with LIS3DSH sensor using I2C protocol. I applied procedures on STM32f manual. But it didn't work. I wanna just receive x axis value. According to this, The GPIOD-12 will be on if it is less than 20. Maybe ı could not realise its...

VAtab.1 by Associate II
  • 1721 Views
  • 3 replies
  • 0 kudos