cancel
Showing results for 
Search instead for 
Did you mean: 

Hi, i am using STEVAL STWINKT1 dev Kit. I need to transmit the MLC value of the ISM330DHCX sensor in real time to the AWS cloud. In the various demos there is no reference to this possibility.

DLomu.1
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Eleon BORLINI
ST Employee

Hi @DLomu.1​ ,

please note that the FW that sends the sensor data on the cloud, i.e. the FP-IND-PREDMNT1 function pack, does manage the MLC of the ISM330DHCX.

The only FW running on the STWINKT1 that currently manages this feature is the HSDatalog example (in the STSW-STWINKT01 pack), but in this case data are sent on the SD card or via USB to the logging application.

This because the MLC is designed to run on the Edge, but cannot exclude that the requested feature will be implemented in the future FW pack and dashboard releases.

-Eleon