MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Anomalous acceleration values from some LSM6DSLs: are they damaged?

I've used a number of times LSM6DSL IMU sensors and I never had any problem with them: they are in general very precise and straightforward to use. However, in a recernt pre-production run, some accelerometers provided strange values on one or two ax...

ADi S.2 by Associate
  • 1698 Views
  • 2 replies
  • 0 kudos

Using LIS3DH with VDD only and using VDD_IO for setup only.

Question is if I can use LIS3DH with VDD only (3.3v) , and VDD_IO (1.8v) supply only during configuration ? And in this case, what power use INT1 and INT2 pins ? If possible to run on VDD only with having them working (at least as OD ?).Datasheet is ...

GLuts.1 by Associate
  • 1202 Views
  • 2 replies
  • 0 kudos

Resolved! HOW TO DEBUG BOOTLOADER USING CUBEIDE

hi, I am trying to debug the bootloader which comes with sensortile.box to change it for my requirements. In doing so I want to inspect how it works using debug session. But unfortunately, when starting to debug the session the curser doesn't even re...

MImda.1 by Associate III
  • 1405 Views
  • 1 replies
  • 1 kudos

LSM6DSL Gyro 800Hz Noise

Hello,When configuring the LSM6DSL ( STEVAL-MKI178V1 ) to sample Data at 6664 HZ ( without any digital Filters active, FS= +- 16g, +- 250deg/s ) there seems to be an consistent 1deg/s @ 800Hz noise on some gyro axis. The same signal but stronger ( > ...

0693W000007CTzeQAG.png 0693W000007CU0DQAW.png
JWoeb.1 by Associate II
  • 2038 Views
  • 3 replies
  • 0 kudos

Resolved! About FIFO of gyro sensor I3G4250D

Is it stored in the FIFO when the threshold of the INT1_THS register is exceeded?Or is it stored regardless of the threshold of the INT1_THS register?

HIMAM.1 by Associate
  • 1528 Views
  • 2 replies
  • 0 kudos

LSM9DS1 Gyro drifting while shutdown

I have an application with a LSM9DS1 that is powered up for a few minutes at a time and then shutoff. It might be powered up again for a few minutes within the same day, or be used only the day after or a few days later. The purpose is to get angular...

PRebo.1 by Associate II
  • 1734 Views
  • 2 replies
  • 0 kudos

Resolved! LIS2DE12 generating interrupts at low ODR

I am trying to get the LIS2DE12 to generate an interrupt when shaken. I have connected the INT1 pin to an open drain I/O pin of my MCU. I an get it to generate the desired interrupt with some reliability. However, when it is just sitting still, it ge...

RKeit.1 by Associate III
  • 1674 Views
  • 2 replies
  • 0 kudos

Resolved! LIS2DE12 self test

I am trying to set up a self test process for an assembly including an LIS2DE12. The device works normally when I tilt and invert it. When I try to put it in to self-test mode by writing either 02h or 04h to CTRL_REG4 the readings are the same as wi...

RKeit.1 by Associate III
  • 3565 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.