Question
Unicleo-GUI -FFT size issue
Hi Team,
Customer is using X-Nucleo-IKS02A1 board to test the vibration sensor using vibration monitoring example code. The FFT data of vibration sensor is observed using Unicleo-GUI.
Vibration Monitoring example code works fine with FFT size of 512. But does not work with FFT size of more than 512.
It is observed that the FFT data is not represented in Unicleo-GUI when FFT size is changed from FFT_SIZE_512 FFT_SIZE_1024 in MotionSP_Config.h file.
Please suggest the configuration settings to increase FFT size.
Regards