MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! IIS2DH Anti-Aliasing Low Pass Filter by Design in comparison to IIS3DWB and what are the resonance frequencies of each axis of the IIS2DH?

Hi,so far we want to compare several MEMS accelerometers and their specifications. From ST, two sensors are on our list, the IIS3DWB and the IIS2DH.For the IIS3DWB, the data sheet offers a frequency response curve at page 19 and regarding aliasing th...

FPal.1 by Associate II
  • 3078 Views
  • 6 replies
  • 0 kudos

Resolved! Counter after interrupt request doesn't enable if condition in main

Hello STM-Community,I'm fairly new to STM programming and I use an STM32 microcontroller with STM32CubeMX encountered a weird issue with my functions.I've got an IRQ, which collects data every interrupt. Similair like this:void HAL_GPIO_EXTI_Callback...

crackl1ng by Associate III
  • 2008 Views
  • 2 replies
  • 0 kudos

Resolved! STEVAL-STWINKT1 vs STEVAL-STWIN KT1B

We purchased late in 2020 an STEVAL-STWINKT1.Just learnt that this board has been deprecated and the  STEVAL-STWIN KT1B is instead the recommended reference designCould you please let us know:if we have to stop using the STEVAL-STWINKT1if get it repl...

dsamm by Associate III
  • 2139 Views
  • 2 replies
  • 0 kudos

Resolved! ISM330DHCX - SPI driven by FPGA - some questions

Hi, I want to drive an ISM330DHCX by an FPGA using SPI. Due to the fast operation and the exact timing I can realise this way, a few questions occured.Data sheet fig. 6 details the SPI timing. There is no value given for minimum time for CS=HIGH, i.e...

ASchm.3 by Associate II
  • 3533 Views
  • 6 replies
  • 0 kudos

STM32L452RE SAI microphone connection RX returns 0

I'm trying to get the SAI working in receive mode with a MEMS microphone, but when i try to receive data it only returns 0? Here is the SAI setup:saiHandle.Instance = SAI1_Block_A; // audio block A.   saiHandle.Init.Protocol = SAI_FREE_PROTOCOL; sa...

RBamf.1 by Associate III
  • 1823 Views
  • 2 replies
  • 0 kudos

How to read multiple IKS01A03 memory register with DMA over i2c?

Hi,I am currently working on DMA combined with I2C bus. I want to read acceleration data from IKS01A3 with HAL function HAL_I2C_Mem_Read_DMA(). I want to read at 6 different memory registers. How can I use that function to get it work properly? Can I...

LZure.old by Associate II
  • 2058 Views
  • 6 replies
  • 0 kudos

Why acceleration data of LSM303D on the Z-axis doesn't work?

Hi,I have a LSM303D, compass, and acceleration sensor. I can communicate with the sensor, and I get the magnetometer data on all of the axes, unlike the accelerometer. Accelerometer Z-axis data comes "-32760" all the time. I work on stm32f103c8t6Here...

0693W000007BYC6QAO.jpg
AÖzba.1 by Associate II
  • 2232 Views
  • 4 replies
  • 0 kudos

WHO_AM_I register value read as 0xFF

Hello ST Community,I have some hardware samples with LIS2DH12 accelerometer. For all the samples except one, the value of WHO_AM_I register is read as 0x33 (which is expected). However, for one of the samples, it is read as 0xFF. What could be the po...

AB.4 by Associate II
  • 1898 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.