MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Stream sensortile box pro data via USB into Matlab

Hello, I have the sensortile box pro. I have used the algobuilder in the MEMS-studio to configure various data outputs (Acc, Gyr, RotationVector 6x). The sensortile isplugged in with USB. I can see those data coming into the MEMS-studio algobuilder e...

Gawa by Associate
  • 438 Views
  • 2 replies
  • 2 kudos

Problem with Heading Calculation

I'm using ST MotionFX v2.7.1 and have encountered an issue with heading calculation.I'm following the sample code from the document:um2220-getting-started-with-motionfx-sensor-fusion-library-in-xcubemems1-expansion-for-stm32cube-stmicroelectronics #d...

gtk by Associate
  • 404 Views
  • 2 replies
  • 1 kudos

LSM6DSV: Z acceleration values too high by 1g

Hi,I read the LSM6DSV on the STEVAL SMKI239AA using a Raspberry Pi Pico running Circuit Python. The CTRL1 register is set to 0x07 (240 Hz ODR, high performance). My output is converted to m/s^2 and looks like that when I move the sensor board slowly:...

PeterK by Associate II
  • 423 Views
  • 3 replies
  • 0 kudos

LPS22HH absolute accuracy

Helloin the data sheet of LPS22HH the absolute accuracy is  ±0.5 in which range of pressure ? ( 800 hPa to 1100 hPa) ? because i tested some samples in 0.3 bar and 0.5 bar, there big difference between the mesure of LPS22HH and reference (exactly val...

ljm by Associate III
  • 450 Views
  • 1 replies
  • 0 kudos

Resolved! how to use motionfxi

I want to use the motionfx library in the x cube mems1 package for my flight control card and ahrs project, my aim is to obtain roll pitch and yaw values with sensor fusion, but I have not come across an example code for using motionfx. Can anyone he...

Resolved! LPS22HB Absolute pressure accuracy

Hello,in the datasheet of LPS22HBTR the absolute pressure accuracy is between 0. and 1 mBar in the range of 0°C and 65°C .Please have more information about the absolute pressure accuracy in negative temperature ? because i will use it betwen -20°C a...

ljm by Associate III
  • 399 Views
  • 1 replies
  • 0 kudos

ASM330LHH whoiam problem ?

I have asm330lhh acceleration and gyro sensor. I have a problem with communication with spi, when I try my other mems sensors (lis3mdl, lis2dh12) with the same connection line, I get the correct whoiam code, while with the asm330llh sensor I sometime...

H3LIS331DL HP filter clarification

Hello,Can you please explain how the high pass filter work? Can it be disabled?I don't quite understand the difference between the two modes "Normal" and "Reference" (AN5881, 5.1.1 and 5.1.2), is the high pass filter always active, so the sensor does...

MD_0-1742320504656.png
MD by Associate II
  • 8083 Views
  • 1 replies
  • 0 kudos

STEVAL-MKI192V1 (LPS22HH) - 50% failure on delivery

HelloI ordered 10 samples of the LPS22HH pressure sensor evaluation board (STEVAL-MKI192V1). Upon receipt, I noticed that each board was packaged in a cardboard box but without an anti-static bag.I then began taking measurements by varying the pressu...

ljm by Associate III
  • 404 Views
  • 1 replies
  • 0 kudos