2025-03-19 2:59 AM
Hello,
in the datasheet of LPS22HBTR the absolute pressure accuracy is between 0. and 1 mBar in the range of 0°C and 65°C .
Please have more information about the absolute pressure accuracy in negative temperature ? because i will use it betwen -20°C and 0°C
thanks
Solved! Go to Solution.
2025-03-21 1:34 AM
Hi @ljm ,
We can't provide this type of information on ST Community.
If you need data in the negative temperature range you should contact your FAE of reference or the Online Support System at this link.
2025-03-21 1:34 AM
Hi @ljm ,
We can't provide this type of information on ST Community.
If you need data in the negative temperature range you should contact your FAE of reference or the Online Support System at this link.