MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Error when trying to connect STEVAL-STWIN to Azure cloud

I am receiving the following error when I was working through the industrial webinarError: Time:Thu Jun 3 18:09:35 2021 File:C:\nobackup\Code\repo\FP-CLD-AZURE1_New\Firmware\Middlewares\Third_Party\azure-iot-sdk-c_public_preview\umqtt\src\mqtt_client...

JTauc.1 by Associate II
  • 1809 Views
  • 2 replies
  • 1 kudos

Resolved! MIS2DHTR

DRIVER TO ASEMBLY BY MPLAB

IZaba.1 by Associate
  • 1109 Views
  • 1 replies
  • 0 kudos

LSM6DS3 linux driver for ODR of 1666 Hz

Hello STM,looking the the mainline kernel for the IMU line, i see some comments in the code that say the only supported ODRs are that of up to 416 Hz. is it possible to run the sensor in high performance mode with the current linux driver? Is there a...

Weden.1 by Associate II
  • 4340 Views
  • 7 replies
  • 0 kudos

Resolved! NucleoSTM32L152 + X-Nucleo-IKS01A3 Example build problem

Hi to allI'm a newbe for this things.My intention is to use the Intensity Detection application for the this system: NucleoSTM32L152 + X-Nucleo-IKS01A3 with ST32CubeMX version 6.21 and ST32CubeIDEversion 1.61.I downloaded MEMS examples from https://...

Alberto1 by Associate III
  • 2603 Views
  • 3 replies
  • 0 kudos

VEML6075 UVA UVB sensor obsolete already?

This VEML6075 looks fantastic for UVA, UVB, and UV Index sensing, but after release in 2016 is already marked obsolete? Why? I can't find any explanation. Are there any suggested alternatives? I can't find any in some extensive web searching.

BBoye by Associate
  • 7747 Views
  • 10 replies
  • 1 kudos

Why are my HTS221s getting bad temperature values?

 I want to know if anyone else has encountered this, I have multiple HTS221 on different boards, and they all give me different temperature values. They are "working," in the fact that when I put my hand on the sensor the temperature increases, etc, ...

0693W000008ypLHQAY.png 0693W000008ypJBQAY.png
IC.1 by Associate II
  • 6146 Views
  • 15 replies
  • 0 kudos

Resolved! Is anyone can explain me the relation between ODR and bandwith?

Hi all,I'am working with LSM6DSO32 and I would like to understand better the relation between ODR and bandwith. What I understand, ODR is output data rate, this is the time where I can read a packet, for example in page 68 of the datasheet Gyroscope ...

SBaro.11 by Associate III
  • 6971 Views
  • 3 replies
  • 0 kudos