MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! MEMS-Studio FSM on MKI109D

Hi, I have the STEVAL-MKI109D board, on which I mounted the STEVAL-MKI250KA. I would like to implement the free-fall example on the FSM, using data from the ST1VAFE3BX biosensor, using only MEMS Studio. Is it possible to do this without writing firmw...

Luisa_97 by Associate II
  • 686 Views
  • 4 replies
  • 1 kudos

Resolved! SensorTile.Box PRO and STEVAL-MKI168V1

Hi, I have an evaluation board STEVAL-MKI168V1 with the sensor IIS2DH. I was hoping to plug it into the DIL24 connector of the SensorTile.Box PRO and be able to see the sensor's output using the MEMS Studio. This does not seem to be the case. Can som...

msv by Associate II
  • 479 Views
  • 3 replies
  • 0 kudos

LIS2MDL, MAGNETOMETER

Hello, I am using the LIS2MDL development kit. I have two questions. When I measure with two development kits in the same environment, I get different values.Both are 5 cm away from each other and there is no factor that will disrupt the magnetic fie...

AlpoTemi by Associate II
  • 664 Views
  • 6 replies
  • 2 kudos

Compensate for Temperature Effects on IIS3DWB

I’m currently developing a vibration meter device and using the IIS3DWB accelerometer. I want to ensure that my acceleration data is as precise as possible. I’ve read that temperature can affect the accelerometer’s performance, so I’m looking for adv...

LIS3DH tilt angle and shock interrupts + ADC

Hi, First of all, I'm not proficient with embedded C, but I would appreciate any input from you that I could feed to ChatGPT. I've been trying to have the codes generated, but they simply would not produce what I wanted. So I have a LIS3DH IMU connec...

MEMS elements inside an accelerometer (LIS2DH12) get stuck

I have a device which uses an accelerometer (LIS2DH12) to trigger a wake up upon movement. Now I have a few samples on my hand, where this wake-up does not work. The design, configuration, interrupt, etc of the parts work (as validated by other ident...

CF3nXftw by Associate II
  • 491 Views
  • 2 replies
  • 0 kudos