MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LIS2DTW12 linux driver

Hi ST experts, Is there any linux driver library available for LIS2DTW12? Where can I find the related information/document? Thanks.

STLearner by Associate III
  • 400 Views
  • 2 replies
  • 3 kudos

Resolved! steval-mki109d with steval-mki245KA standalone logging

Hello,I was wondering if it is possible to set the steval-mki109d with steval-mki245KA to standalone.I would like to test the ISM330BX what is happening when rotating. Thus I have set up a kit with a battery pack and I can start up the measurement wi...

Leo0n by Associate
  • 473 Views
  • 3 replies
  • 0 kudos

SensorTile.box PRO - How to achieve low Sleep Mode Current?

I am looking to extend battery life of the SensorTile.box PRO using sleep mode of STM32U5 and disabling the MEMS sensors. Currently I am measuring approx. 8 mA in this configuration, but I would like to reduce current into the uA range if possible.  ...

db123 by Associate
  • 308 Views
  • 1 replies
  • 0 kudos

Resolved! STEVAL-MKBOXPRO has In Bag and Out bag feature

HI, this is Ahilesh Krishna, I am using STEVAL - MKBOXPRO module for my project, I am eager to know whether this module has in bag and out bag feature in it. Which means whether this would indicate whether the laptop is inside the bag or outside the ...

Resolved! LSM6DS, ASM330, ISM330 digitization multiplexing and filtering

Hello,Could you please confirm that in LSM6DS, as in ASM330, as in ISM330, the low pass gyroscope filtering LPF2 cannot be bypassed and is only driven by ODR_G (no "enable" flag is available for this filtering stage) ?  Furthermore, the block diagram...

fgs by Associate II
  • 406 Views
  • 2 replies
  • 0 kudos

Resolved! Recording Temperature with MEMS Studio

Hello,I wish to test the IMU LSM6DSV, using STEVAL MKI239A and STEVAL-MKI109V3 Motherboard. In the past I've used Unico-GUI, where I could save to file not only inertial sensors' readings, but also temperature. Moving to MEMS Studio, I can no longer ...

Resolved! How to use AH_QVAR on STEVAL MKI250KA

Hi, I have STEVAL MKI109D, on it I mounted STEVAL MKI250KA. I would say if I could use QVAR Swipe Electrode mounted on STEVAL MKI250KA for reading Qvar signal. It is possible?

Luisa_97 by Associate II
  • 403 Views
  • 3 replies
  • 0 kudos