2025-05-16 3:13 AM
Hello,
Could you please confirm that in LSM6DS, as in ASM330, as in ISM330, the low pass gyroscope filtering LPF2 cannot be bypassed and is only driven by ODR_G (no "enable" flag is available for this filtering stage) ?
Furthermore, the block diagrams in the corresponding datasheets suggest that a single ADC (ADC1) is used to digitize the three axes of the gyroscope. Could you please confirm that digitization is indeed multiplexed in these products ?
Thank you by advance for your help.
Solved! Go to Solution.
2025-05-26 3:16 AM
Hi @fgs ,
The LPF2 is not configurable and the cutoff frequency depends on the ODR_G.
There are 3 different ADCs to digitize the three axes of the gyroscope.
2025-05-26 3:16 AM
Hi @fgs ,
The LPF2 is not configurable and the cutoff frequency depends on the ODR_G.
There are 3 different ADCs to digitize the three axes of the gyroscope.
2025-05-26 5:04 AM
Thank you !