2025-05-09 6:19 AM - last edited on 2025-05-29 1:22 AM by Andrew Neil
Hello Team,
We are using the Qualcomm QCS6490 chip set running Android 13 on our custom board.
As part of our project, we have integrated the LSM6DSOTR sensor, which is connected to the DSP pins via the I3C interface. Based on our discussion with the Qualcomm team, we understand that we need to update the JSON configuration files for the LSM6DSO sensor to reflect changes such as soc_id and bus_type.
Although our sensor is part of the PVL, we understand that for all non-POR sensors, the OEM is expected to coordinate with the sensor vendor to obtain the following:
SEE-compliant driver source code
JSON configuration file(s)
Test results, including the Driver Acceptance Checklist validated with the same driver source and registry settings
To proceed with the sensor bring-up, we kindly request the relevant JSON configuration files for the LSM6DSOTR sensor.
Thanks,
Ronak
Solved! Go to Solution.
2025-05-29 1:18 AM
Hi @RGohil
At these links you can find Linux/Android drivers that are publicly available:
If you need additional support, however, I recommend contacting your local FAEs
2025-05-29 1:18 AM
Hi @RGohil
At these links you can find Linux/Android drivers that are publicly available:
If you need additional support, however, I recommend contacting your local FAEs