Resolved! What is STE150N10 replacement?
Hello, did ST ever made a STE150N10 direct (Drop in) replacement?if so, what would be the partnumber? thanks
Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
Hello, did ST ever made a STE150N10 direct (Drop in) replacement?if so, what would be the partnumber? thanks
Hi ,After downloading the stm32f401 disco demo .hex file to the board, the accelerometer functionality is not working after pressing the user button as per the readme instructions. It means the LSM303dlhc chip is damaged.So to confirm that, will you ...
Hello,I'm using nucleoF446RE with X-NUCLEO-IKS01A2. I read data from sensor (LSM6DSL and LSM303AGR) and with MotionFX library I get rotations, but there are some problems.At beginning, if I don't rotate the board, the z-axis rotation is different fr...
I am trying to read the WHO_AM_I register in LSM6DSOX in that register value is (0Fh) and fixed value is (6Ch) but I am getting 0x00 I don't why can you help me regarding this
we want to use VL53L3CX however its driver is too large for MCU, we like VL53L1X Ultra Light Driver idea, is it possible that ST can provide ULD for VL53L3CX ?
Hi,I have a problem with reading the data from accelerometer LSM303DLHC using stm32f401 uc.Here is the code snippet I have extracted from the demo .I was also following the datasheet.int main(void){ GPIO_InitTypeDef GPIO_InitStruct; RCC_AHB1PeriphClo...
I Have configured as shown in the picture , How should I enable the Virtual Com port,. My intention is evaluating all the sensors and push the data to Virtual COM Port. I am writing program for I2C_TempSensor - STTS22H , for that I have configure fr...
Hi Team,Am presently looking for GPS + IMU (sensor fusion) module in STM, what is the best GPS + IMU module and why ? Is sensor fusion algorithm is used in IMU module, if not which algorithm is used in that module, please suggest me best Dead reckoni...
Hi, I'm working on a prototype device. It is very compact, battery powered and has a motor inside. I want to know if the offset can be set (during production) to compensate a very strong magnetic field and still be able to detect earth magnetic fi...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.