MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to stream data through serial port

Hi, I have purchased an STEVAL-MKI109V3 and the STEVAL-MKI207V1 (ISM330DHCX)I followed the instructions in section 4 in dm00331058-stevalmki109v3-professional-mems-tool-motherboard-for-mems-adapter-boards-stmicroelectronics.pdf to stream the dataIf I...

0693W00000DqPWNQA3.png 0693W00000DqPWSQA3.png
NAlwe.1 by Associate
  • 1813 Views
  • 2 replies
  • 0 kudos

Not able to read auxiliary sensor data

Hello,      We are interfaced the nrf52811 with LSM6DSO32 through i2c and LSM6DSO32 is connected to Auxiliary(Temperature MAX30208) sensor through mode 2 connection.here I am able to read the chip id but not able to read the actual temperature data.a...

Resolved! STSS22H No stretch one-shot timing

I want to readout the STSS22H, without any polling or I2C clock stretching. I want to use the following sequence:Send soft reset commandSend one shot command Release I2C bus for other processes to useWait for the maximum conversion time of the one-sh...

allard by Senior
  • 2666 Views
  • 4 replies
  • 0 kudos

Resolved! LSM6DSOX read register

we are trying to configure LSM6DSOX in high-performance mode. Following configurations are done on the sensorODR --> 6.66khz(high performance mode) and G-Range --> 16gRegister addr(CTRL6_C) --> XL_HM_MODE --> value(0x00)Register addr(CTRL6_XL) --> XL...

Sprem.1 by Associate III
  • 3336 Views
  • 9 replies
  • 0 kudos

Resolved! Linux device issue with STEVAL-STWINCSV1b and cli_example

I'm at a loss to figure out this issue with this sensor box, STWINCSV1b. I can get almost all of the applications to build, run and install, I can send the sensor data to the SD files and stream via USB to a terminal and get the BT and WiFi to work. ...

TJM by Senior II
  • 1746 Views
  • 3 replies
  • 0 kudos

Trying to program STEVAL-IDP005V2

Hello,I'm trying to program the STEVAL-IDP005V2 with the stlink mini v3.The problem is that i don't have any power on the board.The St-Link V3 mini is powered by USB, and the power don't go to the STEVAL board.Even when i try to power it through the ...

LMarg.1 by Associate II
  • 2010 Views
  • 3 replies
  • 1 kudos