MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Steval-STWINKT1B - Where is all the power going?

On the STEVAL-STWINKT1B board, and using the HSDatalog firmware, it uses about 60mA in idle state. I have disconnected the sensors, and the uC, and turned off the SD card power lines, but it's still at around 2mA. Does anyone know where this power ...

LWeir.775 by Associate II
  • 2923 Views
  • 6 replies
  • 0 kudos

Resolved! How to configure AcousticBF library for PCM mode?

Are here any example projects on how AcousticBF library should be configured exactly for PCM mode? There are plenty of examples for PDM mode configuration, but none for PCM, which is frustrating, since the documentation on this library is not very ex...

PIvan.9 by Associate II
  • 2230 Views
  • 2 replies
  • 0 kudos

LSM9DS1 WHO_AM_I REGISTER (0x0F)

Hello, I have difficulties to get value of 0x68(IMU) and 0x3D(Magnetometer) from LSM9DS1 WHO_AM_I Reg 0x0F. I did on custom made board with STM32L083RZ and use I2C communication to LSM9DS1. I am using I2C3 PortC pin 0 and pin 1. The SDA&SCL are both ...

ABin .1 by Associate II
  • 2349 Views
  • 2 replies
  • 0 kudos

Resolved! VL53L1x People Count by using Interrupt method

Dear Team,We are using VL53l1X in our application to detect people leaving and entry, we got 5 vl53l1x breakout boards from one of my distributors for prototyping.People count programming working without any issues when using it in polling/continuous...

MMari.2 by Associate
  • 1602 Views
  • 1 replies
  • 0 kudos

LSM6DSO pedometer interrupt setting

Hello,I am using LSM6DSO sensor to do a pedometer. I use the official interrupt signal to control the step update like the following sentence.int1_route.emb_func_int1.int1_step_detector = PROPERTY_ENABLE;But I found the interrupt signal always has so...

JXiao.1 by Associate II
  • 1644 Views
  • 2 replies
  • 0 kudos