cancel
Showing results for 
Search instead for 
Did you mean: 

In the datasheet of vibration sensor I can read there is possibility to use also I2C but you showed only SPI on the slide, is I2C supported at all ?

Pasi MYLLYMAKI
ST Employee
 
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Vladimir JANOUSEK
ST Employee

SPI is the recommended interface because it is faster and therefore has higher throughput possible compared to I2C. IIS3DWB is generating 1.3Mbps so SPI can easily handle, I2C could cover only one sensor axis. In webinar slide we highlighted SPI interface for this purpose, although I2C is available as written in datasheet.