MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

trying to interface with an HX711 load cell amp

The HX711 requires the MCU to send an exact number of clock pulses to capture a 24 bit value, then the clock signal must remain low until the HX711 indicates its ready to transmit again, using the data line. I tried to use a GPIO pin to generate the ...

GrantW by Associate II
  • 17836 Views
  • 28 replies
  • 0 kudos

POSITION ESTIMATION

I am working with DatalogFusion application and I can see the parameters quaternion, rotation,gravity,linear_acceleration,...Assuming the errors of this kind of measurements, Wich is the best option to estimate the 2D position for a vehicle, using t...

RBAGU.1 by Associate II
  • 1170 Views
  • 1 replies
  • 0 kudos

Resolved! STEVAL-STWINKT1 ML ON Microprocessor not ISM330DHCLX

I have a STEVAL-STWINKT1 board and I want to create a ML algorithm for the board to conduct predictive maintenance. However, I want my ML algorithm to run on the microprocessor and not on the ISM330DHCLX sensor. This is because, I realized that the I...

NRaha.1 by Associate II
  • 1424 Views
  • 1 replies
  • 0 kudos

Resolved! Does lsm6dsox provide some pin similar as NRST for hardware reset?

Besides the SW_Reset in CTRL_3 register, can we also do the hardware reset for lsm6dsox through some pins? Or the power gate is only option we can use?The chip worked perfectly on our device, however, in some rare cases, the registers, including whoa...

YYuan.1 by Associate II
  • 1502 Views
  • 2 replies
  • 0 kudos

Question regarding VL53L1X_SetROI()

The function VL53L1X_SetROI() of the VL53L1X ultralite driver also sets the optical center if either X or Y is greater than 10.Is this intended and if so, why ? Neither API description nor header file state anything about this conditional modificatio...

mf101 by Associate II
  • 2562 Views
  • 4 replies
  • 0 kudos

Resolved! Documentation to connect three SensorTiles via bluetooth

Hi,I am working on a project that requires three SensorTiles (STEVAL-STLKT01V1). I am using Raspberry Pi 3B but I am open to use a different device if needed. I am a newbie and need guidance to learn how to do it. Where can I find instructions/docume...

ARami.2 by Associate II
  • 1975 Views
  • 2 replies
  • 0 kudos