MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Does lsm6dsox provide some pin similar as NRST for hardware reset?

Besides the SW_Reset in CTRL_3 register, can we also do the hardware reset for lsm6dsox through some pins? Or the power gate is only option we can use?The chip worked perfectly on our device, however, in some rare cases, the registers, including whoa...

YYuan.1 by Associate II
  • 1571 Views
  • 2 replies
  • 0 kudos

Question regarding VL53L1X_SetROI()

The function VL53L1X_SetROI() of the VL53L1X ultralite driver also sets the optical center if either X or Y is greater than 10.Is this intended and if so, why ? Neither API description nor header file state anything about this conditional modificatio...

mf101 by Associate II
  • 2660 Views
  • 4 replies
  • 0 kudos

Resolved! Documentation to connect three SensorTiles via bluetooth

Hi,I am working on a project that requires three SensorTiles (STEVAL-STLKT01V1). I am using Raspberry Pi 3B but I am open to use a different device if needed. I am a newbie and need guidance to learn how to do it. Where can I find instructions/docume...

ARami.2 by Associate II
  • 2018 Views
  • 2 replies
  • 0 kudos

How can I restart STEVAL-MKSBOX1V1 when running on battery?

I am testing STEVAL-MKSBOX1V1 both connected via USB and running on battery using the mobile app. The device works perfect when connected via USB. However, it behaves in an unexpected way when running on battery. if I disconnect the USB when the app ...

ARami.2 by Associate II
  • 1410 Views
  • 1 replies
  • 0 kudos

Resolved! How to interface with HMC5883L?

Hi. I want to use HMC5833L for my project but I couldn't find any library to be used as a reference. Can someone briefly explain what are the steps needed to read data from the sensor? I have a little piece of code below but it doesn't work.HAL_I2C_M...

M7890.1 by Associate III
  • 3449 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.