MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Best G-Force sensor detail request

Dear all,I need the best accurate G-Force sensor which need to plug inside the cars and trucks for telematics usage which helps to get left turn, right turn, reverse and break event.​Can anyone help me to choose the right ready to go part or solution...

NPate.9 by Associate
  • 1046 Views
  • 1 replies
  • 0 kudos

Resolved! [Closed] Low frequency response of IIS3DWB

I have been characterizing the sub 200Hz characteristic of the IIS3DWB, and we are aware that it is somewhat an uncharted territory.But I was somewhat surprised by my observation when I compared a piezoelectric sensor attached to an IIS3DWB, vibrated...

0693W00000GWdQ1QAL.png 0693W00000GWdPwQAL.png
MAnil.1 by Associate II
  • 3810 Views
  • 4 replies
  • 0 kudos

Resolved! LPS22HB I2C communication error due to pin3 ?

Hello,We are developing a STEM-based educational product. We have just received our initial test PCB for V2.In our PCB for sensing the pressure, we have used an LPS22HB pressure sensor, I am attaching the circuit diagram used for the LP22HB in the PC...

0693W00000GVy7rQAD.png 0693W00000GVy7wQAD.png 0693W00000GVy8VQAT.png 0693W00000GVy8fQAD.png
DBhav.1 by Associate II
  • 2204 Views
  • 2 replies
  • 0 kudos

Tap detection in low power for LIS2DS12

LIS2DS12 has Tap detection functionality. The ODR (output data rate) has to be >=400 Hz is stated in the datasheet. In low power mode ODR of 400 Hz en 800 Hz are supported (10 bit) resolution. Is Tap detection supported in low power mode? I cannot f...

Lama by Associate III
  • 1536 Views
  • 2 replies
  • 0 kudos