MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Dear ST Community, I am currently trying to setup a Finite State Machine (FSM) for the LSM6DSO32. Is there somewhere an example?

I'm using the NUCELO-G071RB with the STEVAL-MKI215V1. I tried to use the example code for the LSM6DSO available on github: https://github.com/STMicroelectronics/STMems_Standard_C_drivers/blob/master/lsm6dso_STdC/examples/lsm6dso_fsm.c, since I did no...

THäck.1 by Associate II
  • 3326 Views
  • 4 replies
  • 0 kudos

LIS2DW internal Anti-Aliasing filter 1. what order of filter is Anti-Aliasing filter? what's the cutoff frequency of attenuation band? What is the attenuation in the stopband?what's sample rate of internal ADC?

Backgroud: i'm hardware engineer and work for SKF. we used your Lis2DW in our product to test speed of metro.Issue: we found some noise siganl or high Freq. aliasing add in collected data in low frequency. In LIS2DW user guide manual, i find some dec...

vwu.11 by Associate II
  • 3177 Views
  • 4 replies
  • 0 kudos

[lis2dh12/lis2dw12] INT1 signal too low/no signal output

Hi guys,I am currently working on a project with lis2dw12 tap and orientation interrupt. I have come across an issue of INT1 output.I have tested the INT1 output signal with the code below:#include "lis2dh_reg.h"   void lis2dh_int_test(stmdev_ctx_t d...

wai.1 by Associate
  • 1360 Views
  • 1 replies
  • 0 kudos

I have edited the real-time 'DataLog' application provided in STSW-STLKT01_V2.5.0 to include the MotionDI_update function. However, my code hangs after I get the tilt and acceleration values for the first time. How to solve this?

int main(void) { HAL_Init();   /* Configure the System clock to 80 MHz */ SystemClock_Config(); MX_GPIO_Init(); MX_DMA_Init();   MX_CRC_Init(); MX_RTC_Init();   MotionDI_Initialize(&freq); /* Optional: Get version */ //...

QAbba.1 by Associate II
  • 1418 Views
  • 1 replies
  • 0 kudos