MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

IIS3DWB acceleration sensor data is strange

y-axisz-axisI am using IIS3DWB to collect the vibration data. When the chip is stationary, the z-axis should be affected by gravity and output 1g, but. But the actual data is that 1g data will often appear on the y-axis data, and the z-axis will bec...

0693W00000NpLHlQAN.png 0693W00000NpLMbQAN.png
YRu.1 by Associate
  • 782 Views
  • 0 replies
  • 0 kudos

LSM6DSO bulk read

Hi,I've configured the LSM6DSO with an NRF52. The NRF52 is able to use DMA and to trigger the SPI clock for bulk read in background without incorporating the CPU. But as far as I can see in the datasheet and the example drivers the LSM is not capable...

CWies.1 by Associate III
  • 976 Views
  • 0 replies
  • 0 kudos

LSM6DSM gravity calculation

Hi,I am testing the accelerometer and can see that it also measures the acceleration caused by gravity.Is there a setting or way to filter gravity out from the reading?If there is any calculation, could you please share us the same for with gravity a...

ANaik.2 by Associate
  • 1543 Views
  • 2 replies
  • 0 kudos

IIS2DH INT1 activation for 6D/4D recognition

Hello dear ST community,How can I get activated INT1 for 6D/4D recognition in IIS2DH?I looked in the datasheet for some information but I couldn't find anything.In these design tips for LIS2DW12/LIS2DH12 the 6D interruption is routed in register CTRL...

LSM6DSO gyro outputs when SensorTile.Box module stationary

Hello,I'm in the evaluation stage of LSM6DSO sensor. I've got a SensorTile.Box module and running DataLogExtended.bin firmware and I use Unicleo-GUI to read sensors' data. I'm expecting to get 0 values for the gyro outputs if the module is stationary...

KT by Associate II
  • 1134 Views
  • 0 replies
  • 0 kudos

8kHz Noise with LIS25BA Accelerometer

I see a constant, very strong peak at 8kHz in all signals measured with the LIS25BA accelerometer without any obvious source. The peak is very sharp, so there is probably a coherent signal coupled into the system, and it's not the sensor resonance or...

CupOfTea by Associate II
  • 4785 Views
  • 7 replies
  • 0 kudos