cancel
Showing results for 
Search instead for 
Did you mean: 

Can we fine tune the activity recognition example for MLC available on GitHub?

Eleon BORLINI
ST Employee
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Eleon BORLINI
ST Employee

Absolutely yes, ST offers on GitHub not only the configuration files which can be used to program the sensor for a quick start, but also configuration details (in the README file), and examples of dataset which can be used to generate the final configuration. The configuration can be fine-tuned using new datasets or different MLC parameters.

View solution in original post

1 REPLY 1
Eleon BORLINI
ST Employee

Absolutely yes, ST offers on GitHub not only the configuration files which can be used to program the sensor for a quick start, but also configuration details (in the README file), and examples of dataset which can be used to generate the final configuration. The configuration can be fine-tuned using new datasets or different MLC parameters.