MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Usage of lis2dw12 to detect shaking

Greetings.We are developing a device that will be needed to detect a back and forth shaking motion (not too unlike that of a cocktail shaker), sending a interrupt (we cannot afford to use polling unfortunately) to a MCU every time the device experien...

IFant.1 by Associate II
  • 1226 Views
  • 0 replies
  • 0 kudos

LIS2DW does not work properly

Hi,I am using nRF52805 with LIS2DW.LIS2DW is connected to nRF52805 with general GPIO, not I2C port.I am emulating GPIO to I2C protocol.SDA and SCL pin is pull-up to 100K resistors.After initializing LIS2DW, no need to use I2C bus.But, in this case, s...

Paul.Lee by Associate III
  • 1488 Views
  • 1 replies
  • 0 kudos

Resolved! Unable to read any register on the LIS2DW12

Hi,​I'm trying to interface a nrf52840 DK with a LIS2DW12. I'm using the ST-Eval board for the IMU. ​I'm able to read the WHO_AM_I register and it gives the correct value(0x44). I tried setting the IMU to 100Hz and the high performance mode. When i t...

GTS.1 by Associate III
  • 1899 Views
  • 4 replies
  • 0 kudos

Resolved! ISM303 for Tilt-compensated compass application

Hi, Can we use ISM303 for a Tilt-compensated compass application? When checking the 'Applications' in datasheet, 'Tilt-compensated compasses' is not mentioned in the datasheet of ISM303, but it is mentioned in the datasheet of LSM303, which are both ...

AJame.3 by Associate
  • 1304 Views
  • 1 replies
  • 0 kudos

Resolved! LSM6DSO - not reading back what i've written. SW reset issue.

Hi,I'm trying to configure an LSM6DSO (sparkfun breakout), using a TWIM/I2C bus, master device is a nordic NRF52.For the most part, the communications appear to be working. I'm able to configure an interrupt to respond to a single tap. The interrupt ...

shows.1 by Associate
  • 1602 Views
  • 1 replies
  • 0 kudos

Is possible that the LIS2DW12 accelerometer reports via interrupt pin the Single and Double Tap condition at the same time?

Hi,I am developing an application using the accelerometer LIS2DW12. I need detect the single and double tap at the same time and indicate it to the microcontroller via interrupt pin what condition was detected.I have could detect single tap and doubl...

LIS331HH self-test output change with voltage

We have performed the self test on two prototype boards,as instructed in this post: https://community.st.com/s/question/0D50X00009XkXegSAF/lis331hh-understanding-self-testThe x and y differences are around 135, which is in the range, but on the z axi...

SVozl.1 by Associate
  • 1178 Views
  • 2 replies
  • 0 kudos