cancel
Showing results for 
Search instead for 
Did you mean: 

LIS2DW does not work properly

Paul.Lee
Associate III

Hi,

I am using nRF52805 with LIS2DW.

LIS2DW is connected to nRF52805 with general GPIO, not I2C port.

I am emulating GPIO to I2C protocol.

SDA and SCL pin is pull-up to 100K resistors.

After initializing LIS2DW, no need to use I2C bus.

But, in this case, some current is consumed thru pull-up resister.

I want to reduce the current consumption below 10uA when nRF52832 is in sleep state.

To reduce the leakage current thru pull-up resister, I find current is lower than output mode.

But, in this state, LIS2DW can not generate INT1 interrupt.

I re-config the SDA and SCL to output mode, LIS2DW is still not working properly, no generating INT1 signal.

  1. How can I reduce the leakage current thru pull-up resistors?
  2. Why LIS2DW can not work after SDA and SCL pin re-configuration?

Thank you in advanced

Paul

What is problem?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Paul.Lee
Associate III

I checked no INT1 by oscilloscope