MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LIS2DTW12 control registers do not persist changes

We are trying to integrate the LIS2DTW12 into our project but aren't able to get basic functionality to work correctly. We see the correct value from `WHO_AM_I`, but then all registers are read only - i.e., when we write to the control registers then...

jw56 by Associate III
  • 1977 Views
  • 4 replies
  • 0 kudos

Resolved! problem with motion_GC library

Hi..My name is Anil and i am facing an issue with mems motion_GC library ie.,regarding MotionGC_Update function (&data_in, &data_out, &bias_update); for this function i am providing data.in and trying to get the calibrated data.out but not gettin...

Anil3 by Associate III
  • 5581 Views
  • 10 replies
  • 0 kudos

I have an ST component that I have a question about; specifically the die markings. I was wondering if the markings are authentic to this component given the following information:

1) Part Number: LSM6DS3HTR           2) Date Code: 2125The markings on the die read: 1)   ST, 2014, CGA04A, VA59B  I apologize in advance if this question was posted to the wrong section.At SMT Corporation we are committed to keeping mission-critical...

DCole.1 by Associate II
  • 1809 Views
  • 4 replies
  • 0 kudos

Connection error : STEVAL-STWINKT1B with ST BLE Sensor

Hi, I have a problem about connecting STEVAL-STWINKT1B with ST BLE Sensor application. Bluetooth connection works. STEVAL-STWINKT1 appears in the list.​If I try to use the vibration monitor, WARNING pops up. I can't proceed with the next step .​I wan...

0693W00000Nqm3YQAR.png
wkim.2 by Associate
  • 1130 Views
  • 1 replies
  • 0 kudos

Resolved! SMD code marking reference? (LSM6DS3)

I have a short strip of tape that's supposed to be LSM6DS3's, but the SMD marking code on them is different from the other tapes I have (which where correctly organized and labeled). So, is there a table where I can look up the codes that refer to th...

RMaia by Associate III
  • 7595 Views
  • 4 replies
  • 0 kudos