Skip to main content
YCHEN.3
Visitor II
September 8, 2022
Question

Why is there no 9-axis IMU available for ST now?

  • September 8, 2022
  • 1 reply
  • 2168 views

For absolute orientation estimation, magnetometer serves as an important role to calibrate the angle drift.

However, it seems there is no 9-axis IMU available now.(ST LSM9D... is obsolete.)

However, for low-cost, consuming purpose 9 axis IMU: BNO055 for Bosch and ICM20948 for TDK.

Is there any issue on integration of 9-axis IMU?

Or 6-axis IMU + mag are enough for current application? ​

    This topic has been closed for replies.

    1 reply

    Eleon BORLINI
    ST Employee
    September 9, 2022

    Hi @YCHEN.3​ ,

    you are basically right... the fact is that the most common application platforms don't use 9-axis any more, mainly for the reason of poor overall performances, that can be better achieved with an IMU + magnetometer separately. ST suggestion is to use a 6-axis such as LSM6DSOX and a magnetometer like LIS3MDL

    -Eleon