MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to enable the MLC option for the MKI197V1 in WL55?

Hello, I'm trying to enable the MLC option for the MKI197V1 and I'm having some trouble.The DatalogFusion runs fine when configured for the WL55JC, but what I want is the MLC option that can be seen on the DataLogExtended sample. Any guidance is appr...

hkout.1 by Associate
  • 1027 Views
  • 1 replies
  • 0 kudos

Cannot I^2C to ST-nucleo-IKS01A3 in a normal I2C setting

Hi I recently bought a IKS01A3 and want to do research related to human activities. I already have a nucleo-wb55 with me so basically I just connect them via arduino uno V3 ports and willing to set up I2C communication between those two boards. I kno...

CWang.14 by Associate II
  • 1805 Views
  • 1 replies
  • 2 kudos

Random glitch on I2S recordings

Hello,I'm using an STM32 M4 for recording short audio signals through the I2S interface and I write the PCM to an SD card. To check that everything is fine I have recorded pure tones (1kHz or 2kHz). By doing that I noticed in some recordings (not all...

frnt by Senior
  • 7723 Views
  • 12 replies
  • 1 kudos