MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM6DSLTR high current consumption

Hi,​We found a problem with high current by using LSM6DSLTR.LSM6DSLTR is used to trigger system from sleep mode.​The normal system sleep current is 0.5~0.9mA. The abnormal one becomes 3.25mA.​This issue is related with this LSM6DSLTR IC. When we rep...

LFu.2 by Associate
  • 2327 Views
  • 2 replies
  • 0 kudos

LSM9DS1 - Properties of the filters of the Accelerometer

The possible configurations of the accelerometer filters are clear:While the properties of those filters and what fields in the registers controls them is not clear at all.Ex documentation https://www.digikey.com/htmldatasheets/production/1639232/0/0...

0693W00000UnHONQA3.png 0693W00000Un9vTQAR.png 0693W00000Un9vdQAB.png
kobelev by Associate
  • 915 Views
  • 0 replies
  • 0 kudos

lsm9ds1 minimal configuration

Hello,I have a very simple compass application which needs to poll the magnetometer, accelerometer and gyroscope roughly every 500mS (the board itself has no interrupt lines connected to the lsm9ds1), with the option of powering down for extended per...

DCarr.1 by Senior
  • 1919 Views
  • 2 replies
  • 0 kudos

LIS2DE12 and a buzzer on board

Hi, folks,I'm using LIS2DE12 on the PCB. The purpose: the device should inform the firmware, if the PCB has moved - intruder detection. I successfully programmed the device for INT1 on 6D movement. It works fine in general.On the PCB I have also a sm...