MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Lis2 accelerometer sensor

Hi,​ I am looking lis2dh12 driver initialization with fall interrupt detection.​Please share sample program for understanding.​Regards,Kumar​

Akuma.6 by Associate III
  • 927 Views
  • 0 replies
  • 0 kudos

Resolved! "WHO_AM_I register value does not match the device selected"

My first time exploring with STEVAL hardware. I just received the STEVAL-MKI108V3 mother board, the STEVAL-MKI196V1 sensor board, and installed UNICO GUI 9.13.0 and FW Version V3.11.4. When starting the Unico Program with both "Automatic Port Detecti...

I3G4250D- PLLFILT required to be mounted for gyro to work

Hello, I am using the I3G44250D gyroscope without soldering the capacitors (C1=10nF,C2=470nF) and resistor (R2=10k) indicated for the PLLFILT, by using a configuration in which only the LPF1 filter is applied by default. With this configuration the g...

CMedi.1 by Associate
  • 926 Views
  • 0 replies
  • 0 kudos

Using FP-IND-PREDMINT1 for determining the frequency of vibration

Hello, I am using FP-IND-PREDMNT1 and new to this . From the data website it says it is used for time and frequency domain signal processing and analysis of 3D digital accelerometers with flat bandwidth up to 6 kHz. I wanted to know if is it possible...

PVaaz.1 by Associate III
  • 1750 Views
  • 2 replies
  • 0 kudos

Resolved! What is the accuracy of the LSM6DSO timestamp frequency of 40 KHz?

There does not seem to be anything in the datasheet about set tolerance, or drift over temperature.  https://www.st.com/resource/en/datasheet/lsm6dso.pdfAssume the INTERNAL_FREQ_FINE is unchanged. It has a step size of .15%, so one would presume the...

STEVAL-BLUEMIC-1 recording problem

Hi!I am using the STEVAL-BLUEMIC-1 to do wireless audio recordings, and I am noticing that the recordings get sped up. Is there a fix to this, or a reason why this may be happening?Thank you,Imran

IKalh.1 by Associate II
  • 827 Views
  • 0 replies
  • 0 kudos

How to access STEVAL-STLKT01V1 in STM32CubeMX

I use the following devices and software:STEVAL-STLKT01V1(STEVAL STLCR01V1)ST-LINK/V2/ 01-0STM32CubeIDE 1.9.0STM32CubeMXSTM32CubeProgrammer​I was able to implement SENSING1 on the device, but I can't specify the board on the MX, so I can't train the ...

庫兵.1 by Associate
  • 1106 Views
  • 0 replies
  • 1 kudos