MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I am currently working on an analog vibration sensor I have to recover 5 harmonics with my Stm32wle5jc I would like to know how to do a simple fft without DMA at first then with? because I am a beginner in the field

I tried to integrate an example of fft on my existing code and I have a problem "undefined reference to `arm_cfft_radix4_f32'" knowing that I just put the file arm_math.h and after I also tried to put the library DSP and lib arm_cortexM4lf_math.lib a...

Resolved! What are the typical ODR deviations (Clock deviations) in the ISM330DHCX and other iNEMO Modules and is it somehow possible to connect external clocks?

Hello,In our application we've found quite big differences in ODR between different samples of the ISM330DHCX and also for different modes:For example if setting the ODR to 416 Hz we measure > 440 Hz. Furthermore when only ACC is active the ODR is 44...

MNoll.2 by Associate II
  • 3065 Views
  • 5 replies
  • 0 kudos

How to resolve a STM32CubeProgrammer error: "Error: No STM32 target found!" while using a ST-Link/V2-lsol probe connected to a SensorTile.box eval board via the 20->14 pin adapter?

I have a SensorTile.box eval board connected to a ST-Link/V2-lsol using the 20->14 pin adapter. The ST-Link/V2 is connected to my linux workstation via USB and the ST-Link is seen by the STM32CubeProgrammer application. The SensorTile.box is also c...

dmcph.1 by Associate
  • 1619 Views
  • 1 replies
  • 0 kudos

IIS2DH Temperature data is not updating

I am working with the IIS2DH sensor. I can read all 3 axis data, but when I try to read the temperature I only got zeros. I read the similar forum threads, and I did not find a solution for my problem. I set the TEMP_CFG_REG(1F) to 0xC0, also set CT...

BLuka.1 by Associate
  • 895 Views
  • 0 replies
  • 0 kudos

53L1A1 SimpeRanging printf problem

Hello,I am working on the SimpleRanging example associated with X-NUCLEO-53L1A1 TOF sensor, so I lanched it using the IAR IDE as noted, but I can't read data in the Tera Term ( nothing is shown on the terminla) although I checked the IAR livewatch an...

WYous.1 by Associate III
  • 1580 Views
  • 2 replies
  • 0 kudos