MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

PDM microphone glitch at beginning of the recording

Hello,I'm using the IMP34DT05 microphone using the I2S interface. I'm sampling at 22kHz but I have a problem when I look at the recording saved on micro SD. In the first part of the audio, I see a glitch and then an exponential decay of that spike (s...

0693W00000aIChgQAG.png 0693W00000aIChvQAG.png
frnt by Senior
  • 10427 Views
  • 13 replies
  • 0 kudos

What could cause the LPS22HH boot phase to never finish?

I am evaluating the LPS22HH for a product, but the device acts a bit unreliably. After power-on, sometimes the BOOT_ON bit in INT_SOURCE (24h) is never cleared.I wait for at least 500ms before checking the BOOT_ON bit, so that should be plenty of tim...

jopuc by Associate II
  • 1218 Views
  • 1 replies
  • 0 kudos

Question about LPS22HH: about POR

I read document AN5209. This said " VDD must be lower than 0.2 V for at least 10 ms during power-off sequence for correct POR. (3.1 Figure 2)"If POR did not finish correctly, is there the possibility to be read the un-correct data?

TOMY.OKA by Associate II
  • 1891 Views
  • 2 replies
  • 0 kudos

Could not read and write the ISM330DLC each 10ms period

Dear ST Hello,I am trying to use the ISM330DLC 3D accelerometer and gyroscope with the stm32F329Discovery board and I am facing some problems when I want to read and write all the registers every 10 ms ISR period.I want to try to change the registers...

Resolved! Lis3mdl Z axis sampling rate

I am trying understand the sampling rate of lis3mdl on the Z axis. The datasheet has only stated on setting the ODR of X and Y but not Z. Only the performance of Z can be set. During testing, I have noticed that the Z axis sampling rate is slower tha...

DGan.2 by Associate
  • 1593 Views
  • 1 replies
  • 0 kudos