User Activity

Hi,We are currently working on a design involving the STM32U5G7VJT6Q microcontroller and would appreciate your expertise in reviewing the power section of our design. I have attached a diagram of the power section for your reference.Could you please ...
Hi, We are using STPIN230 Motor driver in our applicationOur BLDC Motor electrical parameters are:1) Rotor inductance - 0.11 mH2) Terminal resistance - 10.7 ΩQueries we have:1) In our current design we have STSPIN230 connected to motor as follows( in...
Hi,MCU planned to use - STM32U5G7VJT6QPlanning to use PD12,PD13,PE0,PE3,PC7,PE5 as encoder and hall sensor pins as shown below in the image.But these signals are 5V logic. Is it okay if we give 5V to these pins?In datasheet it is mentioned as 5V tole...
Hi, We are using IMU with part number LSM6DSO32TR in our application. Kindly provide us with LSM6DSO32TR details: 1) MTBF(Mean time between failures) 2) FIT(Failure in Time) 3) ROHS compliant (Certificate) I would be a great help!  
Hi, Could you provide any method/code to convert the acceleration values to distance(in cm)? we are able to read the acceleration but we need to know the distance covered as well. How to do it?  
Kudos from