MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! sths34pf80 + lens

Hi!We are working on product that needs to count people on the range of 3-4 meters. We designed dev.board for sths34pf80 and tetsted it with UNICO-GUI. The max range that we are getting is around two meters and therefore it looks that we need to use ...

apallo_0-1693465987293.png
apallo by Associate
  • 5132 Views
  • 6 replies
  • 0 kudos

Resolved! STEVAL-MKI109D Software-Adjustable Power Circuitry

Hi,I'm trying to write custom firmware for the MKI109D. I am currently using an MKI251A adapter board with it for evaluation. How do I set VDD_DUT and VDDIO_DUT to 3.3V on the MKI109D board without using MEMS Studio?   

mki109d_power_supply.png

Marking of LSM6DSVTR

 LSM6DSVTR is marked V3,Does it change the DC format from YWW to Y or another format? What does "4" mean?Thank you. 

VenusY by Associate
  • 363 Views
  • 3 replies
  • 0 kudos

Lsm6dsv320 fsm interrupt issue

I designed a fsm Design for high G application. The odr of high G and fsm are same. The said functionality is generating interrupt when done on eval kit Nucleo board with iks4a1 kit in Mems studio. But when I converted it into header file and loaded ...

rv_08 by Associate II
  • 270 Views
  • 1 replies
  • 0 kudos

Asm330Lhh datasheet clarifications

Hello, I am currently reading the ASM330LHH May 2020 DocID031239 Rev 4 datasheet and its Chinese version: ASM330LHH: Automotive Inertial Module Digital 3D Accelerometer and Digital 3D Gyroscope User Manual. During the design process, I have a few que...

wz2 by Associate
  • 355 Views
  • 1 replies
  • 0 kudos

LIS3DH and LSM6DSV32X on same SPI bus

Hello,I intend to put LIS3DH and LSM6DSV32X on same SPI bus and use different CS lines to address them separately. But when the CS is desactivated, these components activate their I2C engine, therefore leading to possible conflicts of I2C interface o...

Are the LSM6DSVQTR and LSM6DSVTR IMUs equivalent?

On platforms like LCSC and Mouser, an IMU labeled "LSM6DSVQTR" is listed separately from the LSM6DSVTR. On JLCPCB, the LSM6DSVQTR has considerably more stock than the LSM6DSVTR and is eligible for the "economic" PCBA service, unlike the LSM6DSVTR.Do ...