MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Multiple STHS34PF80 on I2C bus

I have an application that requires two STHS34PF80 sensors on the same I2C bus. I tried using N-FETs on the SDA lines to select between them but this doesn't work, not sure why. I will try the 3-wire SPI bus but I am not sure my current MCU API supor...

KWine by Senior
  • 2403 Views
  • 3 replies
  • 0 kudos

Resolved! IMU LSM6DSO FSM Settings

Hello Team ST,I would like to have your guidance on setting a FSM for wrist tilt application. At the moment, we use following FSM settings as per the code here.Link: https://github.com/STMicroelectronics/STMems_Standard_C_drivers/blob/v2.00/lsm6dso_S...

ASoni2_0-1690543414543.png ASoni2_1-1690543657397.png
ASoni.2 by Associate III
  • 1587 Views
  • 1 replies
  • 0 kudos

LSM6DS3TR-C Reading more than one pattern from FIFO

Hi,I'm working with a LSM6DS3TR-C.Currently I've a working app where I configure a FIFO threshold for accel, gyro and timestamp data, and a THS interrupt in INT1.Once the interrupt occurs, I can read all the patterns, one at a time like this:  #de...

Martxel by Associate
  • 1661 Views
  • 1 replies
  • 0 kudos

Resolved! AIS2DW12 Zero-g level offset accuracy, long term

Can anyone tell me how to understand the following parameter out of the AIS2DW12 datasheet.Zero-g level offset accuracy, long term: ± 700mgWhen i use the sensor with a resolution of ± 2g, then I hope there ist not the possibility that the offset will...

dmeise by Associate II
  • 1921 Views
  • 2 replies
  • 0 kudos

LIS2DW12 slow activity detection

Hello everybody,In the AN5038 it is well described how to setup the internal state machine to detect activity, but it has does not fit my need:If I have my  product in my hand, I want detect slow motion in 3 XYZ axes, but if my product is on my desk ...

LSM6DSO - Sensitivity to vibration.

Hi, I am trying to integrate LSM6DSO in an iOT and would like the LSM6DSO raise wake up interruption when iOT is moved (with a normal movement). Now my problem is the following :I programed my interruption and it's run. I can detect the motion on my ...

egeo by Associate
  • 1342 Views
  • 1 replies
  • 0 kudos