MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

IIS3DWBTR power down to wake up process

Hi,We have achieved lowest current consumption(5.5uA) in power down mode as per datasheet with the pin configuration.Now we are trying to wake up from power down mode,By enabling the accelerometer CTRL1_XL register-101_Value ,but still module is in p...

nandhinis by Associate II
  • 1800 Views
  • 1 replies
  • 0 kudos

Resolved! LSM6DSOX SPI read and write protocol in mode 1

Hello! I would like to check if the SPI read and write protocols in mode 1 are the same as those in mode 3 (as suggested on the datasheet). If they're different, may I know what the differences are?Thank you!

Resolved! LIS2DW12 Output Values

Hi experts,I am working with the LIS2DW12 accelerometer and the AN5038 document mentions the function to calculate the output values of the axis. 2g is mentioned, but what about 4g, 8g and 16g? Is the factor "4" the same for all scales?Thank you in a...

TVela1_0-1690469523903.png
TVela.1 by Associate III
  • 1567 Views
  • 2 replies
  • 1 kudos

How to evaluate IIS2ICLX?

I Am building an Inclinometer for tilt sensing with IIS2ICLX and want to evaluate this sensor, so can you Please suggest the Required Material for the same, Like Evaluation board, Mother board required, Software required.*Edited by moderation, please...

DChou.2 by Associate
  • 1668 Views
  • 2 replies
  • 0 kudos

LIS2DH12 reads 0 values and stops generating interruptions

Hello all,We are facing some issue with the LIS2DH12 accelerometer. When the board is powered-up, the accelerometer is booted with the configuration shown below, and in some of the boards, the accelerometer suddenly starts to read 0 in the OUT regist...

LJimé.1 by Associate III
  • 3096 Views
  • 4 replies
  • 0 kudos