MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! ASM330LHH ODR and FS operating procedures.

Can I operate ODR_XL[3:0], FS[1:0]_XL and LPF2_XL_EN of CTRL1_XL of ASM330LHH simultaneously?Should I set FS[1:0]_XL and LPF2_XL_EN first and then set ODR_XL[3:0]?

ggob by Associate III
  • 535 Views
  • 1 replies
  • 0 kudos

LSM303AGR Application Note Clarification Needed

Hello everyone, I am currently using the LSM303AGR's magnetometer and accelerometer. After coding the self-test procedure from the datasheet, and noticed that the number of samples for the magnetometer self-test is way higher than the number of sampl...

LIS3DH Self Test output change too low

Hello,i am trying to run the self test procedure on the lis3dh according to Application Note 3308 but for some reason the  output change (13 lsb) is below the minimum value listed in the lis3dh (17lsb) .If i run the procedure multiple times in a row ...

kweikamp by Associate
  • 494 Views
  • 1 replies
  • 0 kudos

Resolved! LPF filter on IIS2ICLX inclinometer

I would like to implement a low pass filter to filter out noise at frequencies above 2Hz on the IIS2ICLX inclinometer. I would like to have as high an ODR as possible, let's assume 833Hz. My signal has a low frequency, around 0.5Hz.LPF1 will clearly ...

Resolved! ASM330LHH TDA bit not set to 1?

If the TDA bit is not set to “1” even once after 400ms has passed after the sensor is turned on, is it likely that the startup has failed?

ggob by Associate III
  • 574 Views
  • 3 replies
  • 0 kudos

Error in docs for SDDataLogFileX

The SDDataLogFileX example stores the wave file for the digital microphone but in the following docs it wrongly say that it store for the analog microphone :UM2626 at pages 15 (2.1.5) and 30 (2.2.6)FP-SNS-STBOX1_Quick_Start_Guide at page 27

nicolas by Senior II
  • 280 Views
  • 0 replies
  • 0 kudos

LSM6DSOX MLC issue

I am using the MLC of the LSM6DSOX along with the Nucleo-L432KC. I am using the .h file generated from the examples provided by ST (STMems_Machine_Learning_Core\application_examples\lsm6dsox\Motion_intensity\lsm6dsox_motion_intensity).uint8_t LSM6DSO...

Bassem54 by Associate
  • 466 Views
  • 0 replies
  • 0 kudos