cancel
Showing results for 
Search instead for 
Did you mean: 

Order of operation of INT2_CTRL (0Eh) in ASM330LHH

ggob
Associate II

Should INT2_CTRL (0Eh) in ASM330LHH be changed when ODR_XL[3:0] in CTRL1_XL is 0, or should it be changed after being set to non-zero?

1 ACCEPTED SOLUTION

Accepted Solutions
Federica Bossi
ST Employee

Hi @ggob ,

It is recommended to configure INT2_CTRL only after enabling the accelerometer with a non-zero ODR.

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Federica Bossi
ST Employee

Hi @ggob ,

It is recommended to configure INT2_CTRL only after enabling the accelerometer with a non-zero ODR.

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.