cancel
Showing results for 
Search instead for 
Did you mean: 

ASM330LHH ODR and FS operating procedures.

ggob
Associate III

Can I operate ODR_XL[3:0], FS[1:0]_XL and LPF2_XL_EN of CTRL1_XL of ASM330LHH simultaneously?
Should I set FS[1:0]_XL and LPF2_XL_EN first and then set ODR_XL[3:0]?

1 ACCEPTED SOLUTION

Accepted Solutions
Federica Bossi
ST Employee

Hi @ggob ,

You can configure ODR_XL[3:0],FS[1:0]_XL, andLPF2_XL_ENbits of theCTRL1_XLregister in the ASM330LHH simultaneously in a single write operation, as they reside in the same register.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Federica Bossi
ST Employee

Hi @ggob ,

You can configure ODR_XL[3:0],FS[1:0]_XL, andLPF2_XL_ENbits of theCTRL1_XLregister in the ASM330LHH simultaneously in a single write operation, as they reside in the same register.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.