MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Audio USB interface for IM69D130 MEMS Microphones

I recently bumped into an audio USB interface which might fits my needs : the STEVAL-MKI138V1. Indeed, I want to get the audio signals of 4 MEMS IM69D130 microphones onto my PC on Audacity, through a USB audio interface like the STEVAL-MKI138V1. Howe...

Do IMP23ABSU have only MEMS transducer or with any amplifier?

Hello, I want to find some MEMS transducer for microphone for testing our readout IC for MEMS microphone No matter with single or differential output, but the product that I need is the transducer without input buffer, output amplifier and other. Is ...

JKim.38 by Associate
  • 985 Views
  • 0 replies
  • 0 kudos

Resolved! Where to download Unicleo-GUI?

Hello,I have found informations about Unicleo-GUI, and I would like to test it. There are many informations on ST page, but I could not find any link to download it.So where can I download it?Thank you

ANauz.1 by Senior II
  • 3567 Views
  • 5 replies
  • 0 kudos

Resolved! Cannot make accelerometer LIS2DU12 in Sensor.Tile Pro working ?

Hello, I cannot make the LIS2DU12 working in the Sensor.Tile module. I followed the instruction in the AN5648 but I get random values for X, Y, Z. At first, I'm trying to get the readings in normal continuous mode without FIFO. I can connect the devi...

jea74 by Associate III
  • 1835 Views
  • 1 replies
  • 0 kudos

using STEVAL-MKI221V1 adaptor on STEVAL-MKI109V2

Hey, I wanna use MKI221V on MKI109V2, the sensor datasheet says that it's - "Compatible with STEVAL-MKI109V2 by changing resistor settings". Couldn't find any references to what resistor settings are needed and how to implement them, any help would b...

Lev_G by Associate
  • 1084 Views
  • 0 replies
  • 0 kudos

Resolved! Is license needed to use MotionAC libraries

Hi,I am working on project using ZephyrOS and I am trying to link in and use some of your motion libraries.I have successfully linked but the call to MotionAC_GetLibVersion() is returning zero. Looking at assember in my debugger a variable is being t...

capacitive touch with brass metal

Hi,I want to design a capacitive touch application with a brass metal plate. So, i need a sensor that is suitable with brass metal. Is there any advised product for me?

er3481 by Senior
  • 1358 Views
  • 1 replies
  • 0 kudos

SAI1_SD_A Pin Change Issue in Project BVLINKWB1 V2.0.0

Hi All,I am using a P-NUCLEO-WB55 development board in BVLINKWB1_V2.0.0 project. Project ST Link Here: https://www.st.com/en/embedded-software/fp-aud-bvlinkwb1.htmlIn this project, I would like to change the SAI1_SD_PIN from PA10 to PB15 in P-NUCLEO-...

0_PA10_Successfull_Test.png 2_Noisy_Changed_PB15_Pin.png Default_Alternate_Functions.png Desired_Alternate_Functions.png

Configuration wrong and calibration wrong for ISM330DLC

Hello I'm acquiring data from an ISM330DLC per I2C, and I'm having several issues:-I probably have the config wrong several levels. For instance I have the Reg CTRL1_XL configured to 0x75, CTRL2_XL to 0x7C, CTRL8_XL to C8, CTRL7_G to 40, CTRL6_C to 0...