MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Init sths34pf80.c / sths34pf80.h

I am looking to interface with a sths34pf80 on a nucleo-f401re. I want to set up I2C to R/W to the registers and use the included functions.  BSP_I2C1_Init(); uint8_t ret=0; STHS34PF80_Object_t pObj; STHS34PF80_IO_t pIO; STHS34PF80_Init(&pObj); STHS3...

jkutteh by Associate II
  • 2372 Views
  • 3 replies
  • 0 kudos

Resolved! Lis2dh App Scanrate and Speed of Lis2dh

Hello Ladies and Gents,I have following Problem with my App:The Scanrate from given Timer can be in min. 10ms. These ist f=1/0,010=100Hz. So If I configure the Lis2dh to normal or Highres Mode I have a f=1.344 KHz Anybody have an Idea how to increase...

Stv by Associate
  • 1380 Views
  • 2 replies
  • 1 kudos

X-CUBE-MEMS1 PresenceDetection configuration on STEVAL-MKI109V3

I am looking to set up the STHS34PF80 on the STEVAL-MKI109V3 board. I have tried configuring the PresenceDetection mems application. I measured 0 current on jumper 13 and no voltage on STHS34PF80. Are there any tips or suggestions for setting up the ...

jkutteh by Associate II
  • 1041 Views
  • 1 replies
  • 0 kudos

Issue receiving PDM data in STM32L431KBU6TR

I'm currently using MEMS MP34DT06JTR audio sensor with STM32L431KBU6TR Mcu. I'm facing issue in receiving PDM data through SAI/I2S. I have connected one microphone to SAI Block-1 and the L/R pin is grounded. I'm attaching the main.c file and the conf...

Shivam1282_0-1697181446661.png Shivam1282_1-1697181472887.png Shivam1282_2-1697181496286.png

LIS3MDL temperature reading issues

LIS3MDL issues.Issue #1 - There are two 8-bit registers for temperature, and the datasheet says it's two complement, but I don't see any further description of the contents. Is it fixed point 8.8 or is there some division or offset that needs to be d...

hwsw by Associate II
  • 1813 Views
  • 1 replies
  • 0 kudos

Resolved! LSM6DSO Pedometer - Increased Step Count

Hello,I am using the LSM6DSOWTR sensor in a wearable device for step counting.As it's known, the LSM6DSO series features an advanced pedometer, step detector, and step counter.I'm observing many steps counted even when the user is not moving (false p...

KDeli.2 by Associate II
  • 2547 Views
  • 1 replies
  • 0 kudos

Resolved! Compensation in temperature for LIS2DW accelerometer

HelloWe use a LIS2DW12 accelerometer to mesure tilt over a temperature range from -25°C to +70°C.We set the full scale to 2g and chose High Performance mode with Low Noise enabled.We want an accuracy of 0.5°, but we're observing a drift of the order ...

LIS331DL SPI communication issue

Hi guys,   I met a SPI communication issue about LIS331DL. The type of kit board is MKI153. When I tied VDDIO and VDD to 3.3V, the data from chip register by SPI isn't correct. When I only connect VDD to 3.3v, The data  is correct.     The register i...

TommyMao by Associate
  • 2035 Views
  • 2 replies
  • 0 kudos

Using LIS25BA with STM32L4 Nucleo Board

I am using STM32L452RE Nucleo Board and LIS25BA module.I2C works fine. I wish to get accelerometer data through TDM now. I am unable to do so. For now, I am using polling mode. The code I am using is given below and the SAI configuration I am using i...

Arka by Associate
  • 3521 Views
  • 2 replies
  • 0 kudos