cancel
Showing results for 
Search instead for 
Did you mean: 

X-CUBE-MEMS1 PresenceDetection configuration on STEVAL-MKI109V3

jkutteh
Associate II

I am looking to set up the STHS34PF80 on the STEVAL-MKI109V3 board. I have tried configuring the PresenceDetection mems application. I measured 0 current on jumper 13 and no voltage on STHS34PF80. Are there any tips or suggestions for setting up the STHS34PF80 mems sensor on the MKI109V3 eval board?

Thanks

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Federica Bossi
ST Employee

Hi @jkutteh ,

Welcome to ST Community!

Can you share with me a picture of your connections?

PIN13 is GND that's why you don't see any voltage. Vdd is on PIN1.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.