2023-10-11 5:03 PM
Hello Ladies and Gents,
I have following Problem with my App:
The Scanrate from given Timer can be in min. 10ms. These ist f=1/0,010=100Hz.
So If I configure the Lis2dh to normal or Highres Mode I have a f=1.344 KHz
Anybody have an Idea how to increase/decrease the Scanrate to geht all the values of interval?
Also I'm bind to USB and the Transactiondelay from max 500ms.
Stv
Solved! Go to Solution.
2023-10-13 1:34 AM
Hi @Stv ,
Welcome to ST Community!
Regarding the timer scanrate, I don't know how to increase or decrease the frequency (it could be a question for the STM32 section, if it involves an STM32).
However, you can bypass this problem using the FIFO of the sensor: you activate the FIFO with the ODR at 1344Hz, and you read all the queue when the timer triggers.
If this helps you, please mark my answer as "Best Answer" by clicking on the "Accept as Solution" button, this can be helpful for Community users to find this solution faster.
2023-10-13 1:34 AM
Hi @Stv ,
Welcome to ST Community!
Regarding the timer scanrate, I don't know how to increase or decrease the frequency (it could be a question for the STM32 section, if it involves an STM32).
However, you can bypass this problem using the FIFO of the sensor: you activate the FIFO with the ODR at 1344Hz, and you read all the queue when the timer triggers.
If this helps you, please mark my answer as "Best Answer" by clicking on the "Accept as Solution" button, this can be helpful for Community users to find this solution faster.
2023-10-14 12:43 AM
Hi Ms Bossi,
I'll Check it out.
Thanks
BR
Stefan