MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Protection (waterproofing) of LPS22DF

Hello,I hope you are well.Actually I'm using LPS22DF sensor in an environment where there is dust and water.Can you give me some informations and idea on how can I protect the sensor (waterproofing)?Thank you 

ljm by Associate III
  • 2843 Views
  • 8 replies
  • 1 kudos

Resolved! SensorTile.box Pro in Brick mode

I have purchased the SensorTile.box Pro from Mouser, and the device is excellent to work with on coding. I have loaded 0x0000000 with bin file default from F:\ST_SensorTile_Box_Pro\STM32CubeFunctionPack_STBOX1_V1.5.0\Projects\STWIN.box\Applications\D...

RPare.1 by Associate III
  • 11035 Views
  • 10 replies
  • 3 kudos

Inquiry About ST complete evaluation board for Ultrasound Imaging

We are currently working on an ultrasound-related medical application. We need some guidance regarding the ultrasound AFEs for our device.Our application involves generating signals from a depth of 3-10 cm and imaging within a frequency range of 5 to...

aash21 by Associate
  • 1852 Views
  • 2 replies
  • 1 kudos

LSM6DSM interface with STM32L476 in Sensortile board

Hello Team,Recently I bought Sensortile board from ST.  I tried to interface the LSM6DSM gyroscope and accelerometer sensor with STM32L476 microcontroller through SPI half duplex master, but I'm not able to read the device ID or 'Who Am I' register a...

Saranbabu by Associate II
  • 2607 Views
  • 3 replies
  • 0 kudos

Resolved! LIS2DTW12 Power Down question

Hello Everyone!I am working on an application where I have to read the temperature sensor once every minute, and I would like to put the sensor in power down mode when I don't need to read the temperature.Details:1) I am using an STEVAL-MKI190V1 boar...

vard by Associate II
  • 2057 Views
  • 2 replies
  • 0 kudos

Resolved! LSM6DSO and LIS2MDL power consumption on different VDD

Hello everyone, I am in the development phase of a wearbale project including the use of LSM6DSO and LIS2MDL sensors.I found in the datasheets the power consumption related to the two sensors whne powered up at 1.8 V but I didn't find anythong about ...

Resolved! LSM6DSR

I'd like to use SFLP for LSM6DSR. where can I find the examples and SDK? I searched around but couldn't find any. Thanks,

KFCUBE by Associate II
  • 2339 Views
  • 3 replies
  • 0 kudos

Resolved! what are the differences between lsm6dsr and lsmtdso?

Hey, I am using lsm6dsr + nrf 52811.  I found out the driver code provided by ST for lsm6dso in NCS Zephyr driver code. Can I use the lsm6dso driver code for lsm6dsr development? If I can't, what are the differences from lsm6dso for lsm6dsr?Thanks,

KFCUBE by Associate II
  • 2090 Views
  • 2 replies
  • 0 kudos

lsm6dso remove g from acceleration

I would like to eliminate the influence of the gravitational field g from the measurement of accelerationI tried with a high pass filter. Is this the only solution?The problem is that the sensor evolves in space with orientations that vary over time....

chan by Associate
  • 1679 Views
  • 1 replies
  • 0 kudos