MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! IMU sensor

Hi all, Is there any difference between LSM6DSV16x and LSM6DSV16xTR except the packaging?Thanks in advance.

Daya by Associate II
  • 7203 Views
  • 5 replies
  • 1 kudos

Resolved! MEMS IMP23ABSU microphone

Hi, is the sensitivity in the datasheet (-38 dBV +-1) normalized to 1 Pa (e.g. -38 dB re 1V/Pa)?

TomRett by Associate III
  • 1715 Views
  • 1 replies
  • 0 kudos

LSM6DSR self test

I saw there are self test related code in the driver.What's the purpose of self test and when do we need to do self test? Thanks,

KFCUBE by Associate II
  • 1299 Views
  • 1 replies
  • 0 kudos

Resolved! Multiple STHS34PF80 IR sensors nearby each other.

Can several STHS34PF80 IR sensors be used simultaneously, when placed not far from each other, say on the same PCB? If STHS34PF80 infrared sensors are completely passive devices, there should not be any limitations of the distance between them, even ...

aziubin by Associate II
  • 2086 Views
  • 1 replies
  • 1 kudos

Unit of measure for the MEMS IMP23ABSU microphone

Hello, i have searched for this information, but couldnt find it anywhere. Whats the unit of the measured of the MEMS IMP23ABSU mic? I have used the STEVAL-STWINKT1B with the FP-SNS-DATALOG1 from which i created several .csv files that i now need to ...

TomRett by Associate III
  • 11877 Views
  • 14 replies
  • 2 kudos

RMS velocity calculation from accelerometer data

Hello everyone. I'm working on a vibration sensor with RMS velocity output based on measurements from an accelerometer with +-16g maximum acceleration range. There is a simple equation for calculation RMS velocity range and that is : VRMS=Apeak/2*pi*...

MGolm.1 by Associate II
  • 8905 Views
  • 2 replies
  • 0 kudos

LIS2DH12 in molded application

Does anyone know if the LIS2DH12 is ok in a molded application? We have one where we are putting it in a device completely encased in low-pressure molded rubber. The issue we are seeing is that at power up, sometimes the sensor doesn't power up prope...

ande2407 by Associate
  • 1246 Views
  • 1 replies
  • 0 kudos

Horizontal jump measure

I am currently working with a STEVAL-MKI109v3 evaluation card and a STEVAL-MKI217v1 module. I am using UNICO-GUI to collect data from the module, and then processing the data in Python using various filters such as Madgwick, Kalman, and Mahony to enh...

Untitled.png
Isse by Associate
  • 1330 Views
  • 1 replies
  • 0 kudos