MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! ASM330LHH TDA bit not set to 1?

If the TDA bit is not set to “1” even once after 400ms has passed after the sensor is turned on, is it likely that the startup has failed?

ggob by Associate III
  • 507 Views
  • 3 replies
  • 0 kudos

Error in docs for SDDataLogFileX

The SDDataLogFileX example stores the wave file for the digital microphone but in the following docs it wrongly say that it store for the analog microphone :UM2626 at pages 15 (2.1.5) and 30 (2.2.6)FP-SNS-STBOX1_Quick_Start_Guide at page 27

nicolas by Senior II
  • 238 Views
  • 0 replies
  • 0 kudos

LSM6DSOX MLC issue

I am using the MLC of the LSM6DSOX along with the Nucleo-L432KC. I am using the .h file generated from the examples provided by ST (STMems_Machine_Learning_Core\application_examples\lsm6dsox\Motion_intensity\lsm6dsox_motion_intensity).uint8_t LSM6DSO...

Bassem54 by Associate
  • 413 Views
  • 0 replies
  • 0 kudos

Resolved! Need confirmation MSL level MPN - LIS2DW12TR

Hi Expert, Good day. Refer to the attached label image. One label shows MSL 1 and the other shows MSL 3 for MPN LIS2DW12TR. However, the Reliability Evaluation Report for this P/N indicates MSL 1. Both labels have the same COO but different MSL level...

How to Customize STWINKT1

Hello everyone. I'm a beginner to STM32 and STWIN. I'm experimenting with the DATALOG2 firmware on STWIN.My question is about customizing this firmware. What I want to do is keep the DATALOG2 functionality as-is, but add an extra feature: when the ac...

Imu by Associate
  • 808 Views
  • 0 replies
  • 0 kudos

LSM6DSV80X gyro offset

I am using the LSM6DSV80X to get roll-pitch-yaw from SFLP and gyro reading. I noticed that the sensor keeps reporting increasing yaw and increasing offset for X axis while at rest even though the data sheet suggests that it should have up to only 1dp...

qkieu_0-1756075772778.png
qkieu by Associate
  • 628 Views
  • 2 replies
  • 0 kudos

STHS34PF80 Presence and motion sensor

 Hello,        In my case, the STHS34PF80 sensor module is powered using I2C communication with the ESP32 module, and I have tested its functionality only up to 2 feet; beyond that, it fails to detect any presence. However, the datasheet indicates th...