MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

IIS2DLPC interrupts not generated

HelloI have been trying to setup 6D orientation interrupt using IIS2DLPC and I am not getting any interrupts on INT1 pin when the orientation changes beyond threshold. For debugging I tried printing SIXD_SRC (3Ah)  and ALL_INT_SRC (3Bh)  registers. I...

KS.9 by Associate II
  • 3553 Views
  • 6 replies
  • 0 kudos

Resolved! NO DFU DETECTED - STWINKT1B

Hi guysI'm pretty new to the ST world. Just got my hands on an STWINKT1B, hoping to dive into its ultrasonic sound detection features. I spent today tinkering with it, trying to wrap my head around how it all works.So, I've got STM32CubeProgrammer in...

MTBF for LSM6DSO32TR

Hi, We are using IMU with part number LSM6DSO32TR in our application. Kindly provide us with LSM6DSO32TR details: 1) MTBF(Mean time between failures) 2) FIT(Failure in Time) 3) ROHS compliant (Certificate) I would be a great help!  

NIVI by Associate III
  • 1400 Views
  • 1 replies
  • 0 kudos

FP-SNS-DATALOG2 and macOS

I recently updated to a macOS and am have downloaded FP-SNS-DATALOG2 function pack and was going to use the HSDPython_SDK to log data from my STEVAL-STWINBX1, however it appears that macOS is not supported, is that correct?  No love for macOS or am I...

WP by Associate III
  • 2046 Views
  • 2 replies
  • 0 kudos

imu data synchronization

Hello, I'm working with the lsm6do. The lsm6dso is configured to 6,67kHz sampling rate of both, acceleration and gyro data. The INT1 pin will be set if gyro and/or acc data is available (INT1_CTRL = 0x03). In my application I'm polling the int1 pin (...

K-laus by Associate
  • 1173 Views
  • 0 replies
  • 0 kudos

LIS2DUXS12 Qvar and Interrupts

Hi all,I am trying to implement the  LIS2DUXS12 into a design and I am wondering if it is possible to still use the interrupts while using the Qvar sensors. Ideally, I need a way to detect when the device is on the human body and also a way to wake u...

Eyurk by Associate
  • 1238 Views
  • 1 replies
  • 0 kudos

LIS2DW12 - Changing FIFO mode from bypass to cont-to-fifo

GreetingsI am running an application where I am using the LIS2DW12 accelerometer. I am using it for classical sampling of acceleration values in cont-to-fifo mode, which works fine. The FIFO is configured with the High pass filter enabled. I now want...

ZAIDS-S23 by Associate III
  • 2254 Views
  • 2 replies
  • 0 kudos

LIS3DH sensor data offset/value problems

We have designed the LIS3DH onto a custom PCBA, and we are seeing some oddities with the sensor readings post manufacturing. The PCBA goes into a two part injection molded enclosure made of ABS, and the two halves are ultrasonically welded together. ...