MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! IMP34DT05 returns only silence

Hi, I am reading from IMP34DT05 (master receive, PDM), and I always receive 0x00 0x7F 0xFF 0xFF ...and 0xFF's, ever after, until reset of SAI (disable-enable). Playing sound into mic has no effect. In debugger, immediately upon SAI enabled, FIFO is f...

deno1_0-1708522103520.png deno1_1-1708522425239.png
deno1 by Associate
  • 1776 Views
  • 2 replies
  • 0 kudos

LIS3MDL magnetometer output becomes noisy after a bit

Dear community,I am trying to detect metalic objects (train axles) that are passing above two LIS3MDL sensors. For this purpose I am using LIS3MDL breakout boards from PololuWhat I notice is that often, what seems randomly, the signal becomes noisy d...

Screenshot 2024-02-08 130041.png
dburgt98 by Associate II
  • 1729 Views
  • 3 replies
  • 0 kudos

Resolved! sths34pf80 + lens

Hi!We are working on product that needs to count people on the range of 3-4 meters. We designed dev.board for sths34pf80 and tetsted it with UNICO-GUI. The max range that we are getting is around two meters and therefore it looks that we need to use ...

apallo_0-1693465987293.png
apallo by Associate
  • 3251 Views
  • 5 replies
  • 0 kudos

lsm6dso Tap detection

I tried running the code present in the github link -  https://github.com/STMicroelectronics/STMems_Standard_C_drivers/blob/master/lsm6dso_STdC/examples/lsm6dso_tap.cfor Tap detection. But in the logs, I'm not able to see the axis/sign, even after ta...

Varsha by Associate III
  • 2001 Views
  • 5 replies
  • 1 kudos

Resolved! lsm6dsox embedded features

Is it possible to execute features such as pedometer, activity/inactivity detection, tilt/tap, with same configuration of ODR, Full scale? How can I include all these features in a single program?Can someone explain this please

Varsha by Associate III
  • 1343 Views
  • 3 replies
  • 1 kudos

lsm6dso double tap

 whenever double tap is detected, I'm getting interrupts for both single tap as well as double tap. currently both are routed to int2 pins. I tried routing single tap to INT1 and the double tap to INT2 pin, to ensure single tap doesn't operate under ...

Varsha by Associate III
  • 1376 Views
  • 3 replies
  • 0 kudos

Resolved! ASM330LHH imu sensor

hello,i have few basic Question regarding accelerometer sensor.1. accelerometer data coming from imu sensor that is 2's compliment data, so should i receive this data in signed integer or unsigned integer? 2. i want to know whatever raw data is comin...

Resolved! About ODR_XL target during inactivity

Hello,I set ODR_XL target during inactivity(INACTIVITY_DUR XL_INACT_ODR_[1:0]), but when I read CTR1 ODR in inactivity mode, it doesn't change to the setting, why?

Yansu by Associate III
  • 1639 Views
  • 5 replies
  • 1 kudos

Resolved! STHS34PF80 T_OBJECT interpretation

Hello,First time posting in this forum!I'm evaluting the STHS34PF80 sensor and went through these materials: Datasheet & AN5867.However, I could not find any information regarding the interpretation of the object temperature (after calculating the si...

tuanh_0-1709090589564.png
tuanh by Associate
  • 1830 Views
  • 1 replies
  • 2 kudos

Thermal Dependence of LPS33HW

We are currently using the ST LPS33HW pressure sensor in an industrial IoT application. I am aware that this product is being phased out, and we have plans to replace it with a different offering from ST. However, right now, we have 100s of these in ...