head tracking
Hi team Is there development board available for Head tracking feature? I have sensor tile box pro also I am able to get fusion output from that, can I get head tracking output from that?
Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
Hi team Is there development board available for Head tracking feature? I have sensor tile box pro also I am able to get fusion output from that, can I get head tracking output from that?
Hi All,I have a prototype pcb with lis2hh12 + stm32 and i want to configure movement detection into the accell but all informations that i found was about ACT_THS (1Eh) and ACT_DUR (1Fh).In my tests accel does not set INT1 (as desired)... Do anyone k...
I need to have a part that goes beyond +/-2000 dps. The new part LSM6DSV32X does just that (4000 dps). I'm hoping that it is software/register compatible with the LSM6DSO line of IMUs. That way I could just replace this part (pin compatible) and u...
I want to test X-Nucleo IKS02A1 board with MEMS Studio. I tried to connect to 4 different boards:-Nucleo F767ZI,-Nucleo F446RE,-Nucleo L053R8 ,-Nucleo WB15CC,I always get the same error:Some device is already connectedWhat can I do. Is this some lin...
HelloIf a device using LIS2DW12 is fixed in a fixed position, will it be affected by the gravitational pull of the sun or moon and will the gravitational acceleration of each axis change?
I have a Nucleo-F401RE and want to interface with the STEVAL-MKI209V1. I've tried the TiltSensing2_IIS2ICLX and AccelCalibration2_IIS2ICLX examples but none of them talk to the UNICO-GUI, Mems Studio or TeraTerm UART. Any leads? Especially on what fi...
Spikes are present in the data coming from the LIS2DH12 accelerometer when placed in a casing, but when it is in the open there are no spikes. Attached is an image of the 3 axis data plotted from the accelerometer when placed on the table with casing...
Dear All,I hope this message finds you well.I am reaching out to inquire about the key differences between the LSM6DS0 and LSM6DS3TR-C sensors. Could anyone kindly provide insights into whether the LSM6DS3TR-C offers superior accuracy compared to the...
Are there any options to reduce the power consumption based upon the configuration I have set so far ?This while still being able to sample at 10Hz 10 bit and using FIFO so that the MCU could stay 'disabled' most of the time.For my project I need the...
Hi everyone,I'm working on setting up an SPI connection between the LSM6DS0x and an MCU. I'd like to clarify the pin configuration for a full-fledged SPI setup to ensure I'm getting the most accurate data.Specifically, I have the following questions:...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.