MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! MotionEC_Initialize generates an error when it is called

Hello,It seems that the library MotionMC_CM7F_wc32_ot_hard.a is missing the called function, here the error :c:\st\stm32cubeide_1.6.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_2.0.0.2021053...

AMais.1 by Associate
  • 2475 Views
  • 5 replies
  • 0 kudos

iis3dwb issue while capturing data max data-rate

Hi,I am trying to capture data from the IIS3DWB sensor at its maximum rate and save it into a buffer of length 8192 (due to internal RAM limitations). I'm using SPI with DMA to interface with the sensor. However, I'm not able to capture the data corr...

Resolved! LSM6DSL: Clarification of CTRL1_XL Register description

Hi ,We need a clarification in the register values of LSM6DSL for configuring g values. Is this the correct values or is it a printing mistake where 16g is given as 01 ,should'nt this value be allocated to 4g .It would be appreciated if you can kindl...

Screenshot 2025-08-13 113214.png
Gouri_k by Associate
  • 354 Views
  • 3 replies
  • 1 kudos

LIS2DU12TR accelerometer

Hi,I am trying to use the LIS2DU12TR's low address that is 0x18 but I keep on encountering issues with not able to read WHO_AM_I and the accelerometer does not work. Can anyone please help me with this?Also, does it support 100kHz I2C bus?Thanks.

PE4A by Associate
  • 795 Views
  • 3 replies
  • 0 kudos

Resolved! Problem with Resetting LSM303AGR sensor

 Hello everyone,I am using I2C to communicate between an STM32F411 Discovery Board and the on-board LSM303AGR sensor. I have already configured it for a 400Hz ODR, normal power mode, and am reading temperature values (around 25°C to 27°C).However, I ...

Trying to make lis2dh sense any rotation

Hi, I was trying to make the sensor sense slow rotation.I read the datasheet and I guess if I set HPM to work as normal mode, and High-pass filter for interrupt 1so CTRL_REG2 should have 0x81,Then I should read the REFERENCE (0x26) register, (accordi...

abdu21 by Associate
  • 148 Views
  • 1 replies
  • 0 kudos

Resolved! ASM330LHH Initialization Procedure

Thank you for your continued support.From your responses, I have made the following initialization procedure for ASM330LHH.POWER ONCTRL3_C <- 0x42(BDU,IF_INC)CTRL1_XL <- 0x9C(3333Hz,8G)CTRL2_G <- 0x92(3333Hz,125dps)INT1_CTRL <- 0x01(Accelerometer dat...

ggob by Associate III
  • 615 Views
  • 4 replies
  • 0 kudos